Technical FAQs

Ask a Question

What to do if the LCD display is showing Battery disconnected error in SRC10KUXI model?

Kindly find the below Solution : 

· UPS is tuned on without connecting the battery system.

· Bad battery is connected i.e voltage is less than 180 V.

· Battery connection might be loose, either from UPS or from battery end.
Was this helpful?
What can we do to improve the information ?