Technical FAQs

Ask a Question

What is the by-pass procedure for ATS48 Soft Starter.

The by-pass procedure for ATS48 soft starter is as follows:
- The current go through the thyristor and start the motor.
- Then when the start is finish the relay R2 close for by-pass.
- then by-pass contactor close so the current goes through the contactor and the current sensor of ATS but not in the thyristor. Also the thyristors are always firing.
 

 
Was this helpful?
What can we do to improve the information ?