Technical FAQs

Ask a Question

What is the heating limitation of ATV71/61 Passive filter.

The heating limitation is :
-> 5°c to 40°C without derating
-> Up to 55°C with current derating of 3% per additional °C.
 
Was this helpful?
What can we do to improve the information ?