Technical FAQs

Ask a Question

What is the flashing frequency of XVBC6B3 Indicator bank.

Flashing frequency is 1 Hz.
The frequency of the flashing 1Hz express the numbers of complete cycles per second, So 1 Hz means that complete flashing cycle is generated 1 time per second. The cycle is composed by OFF and ON state when each one is 0.5 cycle/second.
Was this helpful?
What can we do to improve the information ?