Technical FAQs

Ask a Question

What is the rated insulation voltage Ui of TeSys H Ultra Compact Starters.

The rated rated insulation voltage Ui of TeSys H Ultra Compact Starters conforming to IEC/EN 60947-1, overvoltage category III, degree of pollution: 2 is 500 V.
Was this helpful?
What can we do to improve the information ?