Technical FAQs

Ask a Question

What is the rated impulse withstand voltage (Uimp) of TeSys H Ultra Compact Starters.

The rated impulse withstand voltage (Uimp) of TeSys H Ultra Compact Starters Conforming to IEC/EN 60947-4-2 is 6 kV for 24 V DC control voltage and 4 kV for 110 V - 230 V AC control voltage.
Was this helpful?
What can we do to improve the information ?