Technical FAQs

Ask a Question

What is the degree of protection (IP) of TeSys H Ultra Compact Starters.

The degree of protection (IP) of TeSys H Ultra Compact Starters Conforming to IEC / EN 60947-1 is IP20.
 
Was this helpful?
What can we do to improve the information ?