Technical FAQs

Ask a Question

Does xC60 MCB comply to the Fire Resistance Requirement.

The xC60 CB is based on C60 ,hence it complies with glow-wire test at 960°C according the standard IEC 60695-2-10 and that the raw materials used for the housing of these products comply the tests according the classification I3 / F2 of the NF F 16-101 / 16-102.
 
Was this helpful?
What can we do to improve the information ?