Technical FAQs

Ask a Question

Is it possible to configure BMXNOM0200 module as Slave in X80 drop.

Yes,  we can configure BMXNOM0200.4 module as Slave in X80 drop . For that we must have BMXCRA version as  minimum 2.14 or higher and BMXNOM0200.4 version as 1.5 for proper work in slave mode. 

Refer the attached firmware files BMXCRA312x0SV2.15 and BMXNOM0200V1.5 for ready reference.

Was this helpful?
What can we do to improve the information ?