Technical FAQs

Ask a Question

What are the reference of SFP Socket required for M580 HSBY sync link and its speed.

A selectable SFP socket are Available:
490 NAC 0100 - RJ45 (max. length = 100m)
490 NAC 0201 - Fiber Optic LC Single Mode (max. length = 15km)
 
The connection has a 1 Gigabit Ethernet range
1000BASE‑T Twisted-pair cabling (Cat-6, Cat‑7) 100 meters 
 
Was this helpful?
What can we do to improve the information ?