Technical FAQs

Ask a Question

How to configure bmxnom module as a Modbus slave in Quantum x80 drops.

To configure the BMX NOM 0200.4 as a modbus slave / master in a x80 drop, you have to:
  • Use the following firmware versions:
    • BMX CRA 312 10: SV ≥ V2.10
    • BMX NOM 0200: SV ≥ V1.4
  • Interlink a 140 NOC 78• 00 to the Quantum 140 CRP 312 00
The 140 NOC 78• 00 manages the routing of the Modbus frames between Ethernet I/O and the CPU. 
Was this helpful?
What can we do to improve the information ?