Technical FAQs

Ask a Question

How to convert a pl7 application to Unity pro

Converting a PL7 application into a Unity Pro application requires the following:
  • the application to be saved using PL7 ≥V4.3 software, all PL7 applications earlier than version 4.0 must be updated, before being converted into a Unity Pro application. To update a PL7 application, execute the following actions running PL7 ≥V4.3.
  • a level TSX ••• ••4 application processor,
  • the application, as well as the sections, functional modules and dfb's it contains to be unprotected,
  • the application source file to be exported and saved. (.fef)
Below steps for saving the pl7 application :-
 
1 Choose the Open command from the File menu.
2 Select the hard disk and/or directory containing the file to be opened.
3 Select the file to be opened; the name of this file then appears in the File Name field.
4 Confirm with Open.
5 In the Application Browser, double-click on the Configuration directory.
6 Double-click on the Hardware configuration sub-directory.
Result: The Configuration screen appears.
7 Select a version TSX ••• ••3 processor that is compatible with your application from the drop-down menu in the top left-hand corner of the Configuration screen.
Result: The Change Processor screen appears.
8 Confirm your selection with OK.
9 Select the Save command from the File menu.


To export a PL7 application, execute the following actions running PL7 ≥V4.3:
 
1 Select the Export application command from the File menu.
2 Select the disk and/or directory where the file must be stored.
3 Enter the file name in the Name field.
4 Confirm with Save.
Was this helpful?
What can we do to improve the information ?