Technical FAQs

Ask a Question

How to Enable the power-saving function in Back-UPS BR1500GUXI ?

Kindly follow the below steps to Enable the power-saving function in Back-UPS BR1500GUXI :

Press and hold MUTE and DISPLAY simultaneously for two seconds.
The Back-UPS will beep to indicate that the feature is enabled. The leaf icon on the display will illuminate.
Was this helpful?
What can we do to improve the information ?