Technical FAQs

Ask a Question

It is possible to set output voltage in UPS SRC1KUXI ?

Yes,to set the output volatge follow below steps.
Select the ‘Configuration’ option from Main Menu and enter on it.
• Select ‘UPS settings’ and click enter on it.
• Select ‘UPS output voltage’ option.
• Press down ‘arrow button’ to select the desired output voltage(220/230/240) and enter on it.
Was this helpful?
What can we do to improve the information ?