Technical FAQs

Ask a Question

How to set Low battery state indication in UPS SRC1KI-IN ?

The UPS will emit audible alarm when the actual run time reaches the limit set by the end user. The audible alarm will emit only when the UPS is working in
battery mode. To set low battery Alarm indication follow below steps 1)Go to Main menu select 'configuration' press enter  2)Select 'Low battery
state indication '  press enter 3)Select option 2 min, 5 min,8 min, 11 min,14 min, 17 min,20 min, 23 min  according to your requirement.
Was this helpful?
What can we do to improve the information ?