Technical FAQs

Ask a Question

What is the forms and IP rating available in Blokset type D and what is Maximum Distribution BusBar rating.

Please find below details related to Blokset D type

Forms : 1/2B/3B/4
IP Protection : IP20, IP31, IP42, IP54
Distribution Busbar Rating : upto 3200A
Was this helpful?
What can we do to improve the information ?