Technical FAQs

Ask a Question

What are the data rate settings available in Smartlink and whether the communication speed will wary for serial devices.

Data rate setting available in Smartlink are 9600 & 19200. The Modbus network communication speed is same for all serial connections. It is imposed by the
lowest communication speed of a slave device.


 
Was this helpful?
What can we do to improve the information ?