Technical FAQs

Ask a Question

Do we need to be present physically at the device for the firmware upgrade or can it be managed remotely as well?

The firmware upgrade can be done remotely on the network online. Make sure FTP port is opened for the rPDU IP address and reachable via FTP.
Was this helpful?
What can we do to improve the information ?