Technical FAQs

Ask a Question

How to upgrade the firmware of AP8XXX rPDU ?

If you have a Windows computer, you can use the firmware executable to upgrade the firmware. Download the firmware executable file on your Windows PC.

1. Click on the firmware executable once the download is complete. The executable will proceed to unzip firmware files and extract them. You can specify the location where you want the firmware to download to.

2. Once the firmware has been saved, the executable will prompt you to enter the IP address and username and password. You can enter those and press Upgrade Now. 3. The firmware executable will then begin the upgrade process. This process may take as long as 5-7 minutes to finish. Once finished, close the executable.
Verify that the firmware upgrade was successful.

Log into the web interface and go to About->Network menu. The updated firmware should be listed on this page. Alternatively, verify via Telnet, SSH, or local console connection on the main page after log in.
Was this helpful?
What can we do to improve the information ?