Technical FAQs

Ask a Question

How to connect 12 V external batteries with BR1000GUXI ?

Adhere to all national and local electrical codes.
Do not connect the positive and negative terminals on a single battery. Doing so
can cause the terminals to short and may cause a fire hazard.
Connect no more than two external 12 V batteries in series. The batteries must be
of the same Ah capacity

Please follow below steps:
1. Remove the safety covers on the battery terminals.
2. Use the short jumper cable to connect the negative terminal on battery 1 to the
positive terminal on battery 2.
3. Locate the color coded cable with the 3 pin cable assembly.
Connect the red cable to the positive terminal on battery 1.
Connect the black cable to the negative terminal on battery 2.
Connect the 3 pin connector to the external battery receptacle on the rear panel
of the UPS.
4. Replace the safety covers on the battery terminals
Was this helpful?
What can we do to improve the information ?