Technical FAQs

Ask a Question

How does Master and controlled outlets sockets work in BR1000GUXI ?

To conserve electricity, when the device connected to Master Outlet goes into Sleep or
Standby mode, or turns Off, the Controlled by Master device(s) will shut down as well,
saving electricity.
Connect a master device, such as a desktop computer or audio/visual receiver to the
Master outlet. Connect peripheral devices such as a printer, speakers, or a scanner to the
Controlled by Master outlets
Was this helpful?
What can we do to improve the information ?