Technical FAQs

Ask a Question

What is the procedure to set the threshold in BR1000UXI ?

Setting the threshold : The amount of power used by a device in Sleep or
Standby mode varies between devices. It may be necessary to adjust the threshold at
which the Master outlet signals the Controlled outlets to shut down

Please follow below steps:
1. Ensure a master device is connected to the Master outlet. Put that device into
Sleep or Standby mode, or turn it OFF.
2. Press DISPLAY and MUTE simultaneously and hold for six seconds, until the leaf
icon flashes three times and the Back-UPS beeps three times.
3. The Back-UPS will now recognize the threshold level of the Master device and
save it as the new threshold setting.
Was this helpful?
What can we do to improve the information ?