Technical FAQs

Ask a Question

What is maximum allowable make current (without break condition) in DC24V (DC-13 utilization category) circuit of CAD* relay.

The “Short time rating permissible “ is the answer i.e. 140 A for duration of 100 ms
Was this helpful?
What can we do to improve the information ?