Technical FAQs

Ask a Question

What are the keyboard shortcuts available with the Configurator and the L500 MV substation supervision system ?

The available shortcuts are as follows:
Ctrl+A    Selects all drawing elements in the active window
Ctrl+C    Copies the selected drawing element(s)
Ctrl+N    Creates a new window
Ctrl+O    Opens a window
Ctrl+S    Saves active window
Ctrl+V    Pastes the content of the clipboard in the active window
Ctrl+X    Cuts the selected drawing elements
Ctrl+Y    Repeats the previous Cancel command
Ctrl+Z    Undoes the previous drawing actions
Ctrl+F2    Language changeover (defined by the language pair used)
Alt+Enter    Shows the properties of the selected drawing element
Was this helpful?
What can we do to improve the information ?