Technical FAQs

Ask a Question

Is it allowed to use high rating detuned reactor (50kVar) with low rating capacitors (30kVar)

No. It is not allowed to deviate from the combination provided in catalog.Detuned reactor impedance is tuned with the capacitor impedance to detune the circuit.
So impedance of 50kvar reactor if used with 30kVar will change the detuning frequency.
Was this helpful?
What can we do to improve the information ?