Technical FAQs

Ask a Question

What is the reference of RC Filter which should be use for achieving ZSI function Between Masterpact and NSX Breaker and what is the procedure of testing ZSI functionality between Masterpact and NSX Breaker.

Reference of RC filter is LV434212 which should be for achieving ZSI function between Masterpact and NSX Breaker and ZSI functionality can be tested using LTU.

Please refer attached file.
Was this helpful?
What can we do to improve the information ?