Technical FAQs

Ask a Question

Bluetooth Port Hangs during Power Chute Business Edition application Installation

The installation of PowerChute Business Edition Agent hangs during automatic detection of a UPS if a Bluetooth® port is enabled. 
Disable the Bluetooth port before installing the Agent or manually select the UPS type and port during the Agent installation.
Was this helpful?
What can we do to improve the information ?