Technical FAQs

Ask a Question

For TM221 controller, is there a method to create a clone of the application in SD card when the application has application protection enabled

In case of application is password protected inside M221, Clone function is blocked and there is no other way to clone application from controller.

What user can do is he can clone the application from the SoMachine Basic software v1.4 and onwards but it is must to have a project.
If project back-up is there then open the project. Go to the Commissoning => Controller Management => Controller Memory Management => Action = Create controller image.
Save this image file to the directory on system of PC or to Controller SD card whichever is feasible.
Check the box, Include firmware if firmware is to be clonned.
By this way image is copied and later it can be copied to the other controller.
 
Was this helpful?
What can we do to improve the information ?