Technical FAQs

Ask a Question

Does Schneider have offer for DP/PA Coupler that can be used with PRM module.

As of now Schneider Electric do not have DP/PA coupler in there product basket. With PRM you may use Segment Coupler (SK3) from P&F. Refer to the below links for more details
http://www.pepperl-fuchs.us/usa/en/15261.htm
http://www.pepperl-fuchs.us/usa/en/classid_1482.htm?view=productdetails&prodid=28138

 All types of couplers are supported:
• Segment coupler
• Gateway-type segment coupler
• DP/PA link

Gateway-type segment couplers are recommended:
• transparency on a software configuration point of view: PA devices are seen as DP devices
• No restriction on PROFIBUS PA data volume
• Support of PROFIBUS DP high transfer rates 

Any third party standard DP/ PA coupler should work, as per TVDA documnet  referance of P&F used & tested. You may explore on website for any other such products. Below link could be of some help

www.vega.com/downloads/ext-BA-EN/PA-Koppler_X_SK1_EN.pdf
Was this helpful?
What can we do to improve the information ?