Technical FAQs

Ask a Question

What is default IP of Wallbox Pro screen and motherboard

Default IP is (screen) and (motherboard).
When the installer change this settings, it has to be done unplugged from the network and with 2 free consecutive IP address.
Was this helpful?
What can we do to improve the information ?