Technical FAQs

Ask a Question

Is it possible to implement local/remote control selection in Masterpact Breaker with Micrologic P/H

Yes. It is possible to implement local (manual)/remote On the “remote control” settings on the Micrologic P/H Communication Setup menu. You can choose either “Manual”or “Auto”. 

On the “Manual” mode, it is not possible control the breaker neither from the FDM121 nor from a remote Modbus device (PLC, SCADA). You can only use the ON / OFF pushbuttons on the breaker front face or the voltage release MX, XF if they’re installed and properly energized. 

On the “Auto” mode, it is possible to control the breaker either from the FDM121 (if the FDM121 control is set “Local”) or from a remote Modbus device PLC, SCADA (if the FDM121 control is set “Remote”)  
 
Was this helpful?
What can we do to improve the information ?