Technical FAQs

Ask a Question

What is the meaning of "I LO ALARM" on VarPlus Logic VL12 display.

The meaning of  "I LO ALARM" on VarPlus Logic VL12 display is that Measured current is too low (less than 15 mA) and as a result all steps are opened in succession.
Was this helpful?
What can we do to improve the information ?