Technical FAQs

Ask a Question

How to reset KWh in PM8240 meter.

In PM8240 , the device framework is the same as that we can see on the ION7650 and similar devices (i.e. the ION8600, 8650, 8800, 7600 etc.) and these devices reset to zero at the threshold that is set. 

By default, the framework resets to zero at the default threshold which is 10 000 000 kWh. 

 
Was this helpful?
What can we do to improve the information ?