Technical FAQs

Ask a Question

What type of insulation is for BMXFCW303 cable,

The cable sheath for BMXFCW303 is made up of PVC compound according to UL Style 2919 ,80 degree celcius, 30 V.

This cable is complied for Flame resistance according to IEC60332.1 and VDE0472-804 Test B.

Was this helpful?
What can we do to improve the information ?