Technical FAQs

Ask a Question

Can we use ABE7CPA412 telefast module for BMXART0814 Module wiring connection.

Yes , we can use ABE7CPA412 telefast module for BMXART0814.

The TELEFAST ABE-7CPA412 accessory is a base unit used to connect 4-channel analog modules to screw terminal 

For 8 channel module i.e. BMXART0814 module you need to use 2 No. of  ABE7CPA412 telefast module as shown in attached document .
 
Was this helpful?
What can we do to improve the information ?