Technical FAQs

Ask a Question

Can we calculate the position of the sun in Zeliosoft.

Yes, Sun position can be calculated in Zeliosoft with the help of below mentioned to function blocks:

1.       Suntrack

2.       Sunrise/Sunset

Refer the attached document for detail on above function blocks.
Was this helpful?
What can we do to improve the information ?