Technical FAQs

Ask a Question

We are getting message "The request data address is Invalid" while forcing the output channel in test mode for STBDDO3705 module.

This message usually comes when STBNIP2311/STBNIP2212 module is configured at default IP address. 
Once it set to Stored IP the issue will get resolved itself. 

rotary switches set to Bootp - Test Mode ok 
rotary switches set to DHCP - Test Mode ok 
rotary switches set to Stored - Test Mode ok 
'Test Mode' did work if the IP address was the same as the IP derived from the default MAC address. 
Was this helpful?
What can we do to improve the information ?