Technical FAQs

Ask a Question

What is the limitation with PL7 Demo version as compared to licensed version of PL7 Pro

The demo version has almost all of the functionality of the licensed version of PL7 Pro. 

The only differences are:

1) the words "DEMO " appear continuously on the main desktop screen. 

2) You cannot save a new application that you create with the demo version.(although you can use demo files created with a licensed version) 

3)You cannot transfer the application from PLC to PC

4)You cannot import an application.
Was this helpful?
What can we do to improve the information ?