Technical FAQs

Ask a Question

How many TCP/IP master connections can be opened simultaneously over Link 150.


EGX150 (Link150) opens 32 master connections simultaneously over TCP/IP with firmware version "Link150v5-0-23_Firmware_EGX150" as shown in attached snapshot.
Was this helpful?
What can we do to improve the information ?