Technical FAQs

Ask a Question

What is the response time of of Masterpact NT when operating XF release at rated operation voltage

Response time of Msterpact Nt breaker when operating XF release at rated operation voltage i.e. Un is 55 ms with +_ 10 ms accuracy.
Was this helpful?
What can we do to improve the information ?