Technical FAQs

Ask a Question

What is Test Button Operating Voltage Range of 2 Pole 30mA RCCB ID B type

For  2 pole, 30mA RCCB ID B type test button operating voltage range is 160V to 250VAC and for 4 pole 30mA RCCB ID B type test button operating voltage range is 250V to 440V AC.
Was this helpful?
What can we do to improve the information ?