Technical FAQs

Ask a Question

What is the current rating of LRE482.

Current rating of LRE482 is 84A to 135A and current rating adjustment is done using 4 dials options provided on the overload relay.

Please refer attached instruction sheet of LRE482

 
Was this helpful?
What can we do to improve the information ?