Technical FAQs

Ask a Question

What is the purpose of battery saver option in Bx1100Ci-in ?

This feature helps the UPS to offer consistent  runtime during the lifetime of the battery. It increases battery life up to two times. Runtime of the connected equipment will reduce when this feature is enabled. Press the BATTERY SAVER button to activate the battery saver feature. Battery saver LED will illuminate to indicate the UPS is working in the battery saver mode.
Was this helpful?
What can we do to improve the information ?