Technical FAQs

Ask a Question

What is No Load Shutdown in Bx1100CI-in .

The no load shutdown feature works when the Battery Saver mode is enabled and the Back-UPS is in the On Battery mode. The Back-UPS will shutdown if the connected load draws less than 30 W of power for more than 5 minutes. Disable Battery Saver mode if only low power consuming equipment like ADSL-modem or wi-fi router is connected to the Back-UPS.
Was this helpful?
What can we do to improve the information ?