Technical FAQs

Ask a Question

What is the displacement power factor for ATV71 drive.

Displacement power factor, DPF, is the angle between Voltage and the Current at the fundamental line frequency. So in that case, for a drive, the displacement power factor is close to 1.
 
Refer to attached document, which explains DPF is near to 1.
Was this helpful?
What can we do to improve the information ?