Technical FAQs

Ask a Question

How many maximum numbers of ATV600 per 1 profibus loop that is normal practice of Profibus DP.

When profibus network built with ATV600, you should respect and follows the Profibus hardware specification (maximum device per segment, maximum length/ baud rate...). See in attachment.
Was this helpful?
What can we do to improve the information ?