Technical FAQs

Ask a Question

Segment Invalid RIO Drop Error during conversion of Proworx to Unity Pro with Quantum ERIO.

To overcome the Invalid drop error for converted application, follow the below steps:

Right Click on Segment>> properties>>Remote I/O tab>> Set read/write value to 0 or 1.

ERIO will not work with the RIO option and  this remote drop may use in S908 architecture .

You may use IU_ERIO function block  to do Immediate remote drop I/O Access. 
Was this helpful?
What can we do to improve the information ?