Technical FAQs

Ask a Question

What is the part number of Pre-Wired connector for Proximity Switch XS1M18MA230K.

Connector for XS1M18MA230K is 1/2" 20UNF connector type.
You must select suitable reference of Pre-Wired 3-Pin Female 1/2" - 20 UNF connector based on required cable length. Refer to attached document.
For Example:
XZ CP1865L2 (Pre-Wired 3-Pin Female 1/2" - 20 UNF straight connector, cable length: 2m) /
XZ CP1965L2 (Pre-Wired 3-Pin Female 1/2" - 20 UNF Elbowed connector, cable length: 2m).
Was this helpful?
What can we do to improve the information ?