Technical FAQs

Ask a Question

What is the flame resistance of Acti9 C120 MCBs

The raw material used for the case and cover on C120 product comply with glow-wire test at 960 and 650°C according the standard IEC 60695-2-10 and at the fire classification V-2 according the standard UL 94. 
Was this helpful?
What can we do to improve the information ?