Technical FAQs

Ask a Question

What is the rated operational current of LC1F1400 AC-1 at 70 degree.

Please refer the below chart for the rated operational current of LC1F1400 AC-1 at 70 degree :

For ambient temperature above +55°C control voltage must be at Uc. For LC1F2100 the terminals must be fitted with LA9F2100 right-angled connector. 



 
Was this helpful?
What can we do to improve the information ?